Part Number: LM5176
上电后VCC电压只有3.5V
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
Vcc电容是否足够,并尽量靠近芯片Vcc脚?
UVLO电压是否异常?驱动上是否异常?
是否更换芯片是否确认是芯片问题?
是的,我得参数是
Vin = 5.0-40V
Vout = 12.0V
Iout = 6.0A
f=330K
Vin在12-15V之间buck工作正常,超过15V以后,工作模式仿佛进入断续模式,SW1节点电压从方波变成,断续的电压波形,输出电压一直在10V-12之间跳变,一段时间后芯片VCC损坏,最终VCC电压只有3.5V,更换了芯片后VCC正常。
我把功率电感从2.2uH增加到4.7uH,Vin在20V以内可以维持12V输出,超过20V后,又会遇到之前问题,我想问下,补偿,slope电容我都调试过,但是作用不大,请问我该朝哪个方向去检查
HI
直接用webench确认一下电路。
layout严格参考datasheet及说明。