This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R1: Full charge Capacity 充满容量低

Part Number: BQ40Z50-R1

大家好!

    请问BQ40Z50-R1自学习后Full charge Capacity=2354mAh充满容量低是什么原因?

      1、电芯标称:2800mAh    电芯魔力P28A   放电截止电压 :2.5V  充电截止电压:4.2V;

      2、 更新后:Max Error=1%,Qmax Pack=2805mAh;

      3、学习设置:恒流充电:580mA  结束电流:25mA  静置:140Min;   恒流放电:280mA   结束电压:8.6V;

          自学习后 Full charge Capacity=2354mAh充满容量低 、请大家 指点解决办法!!