Part Number: BQ79616-Q1
Other Parts Discussed in Thread: BQ79616
您好:
Bq79616的BAT供电由外部电源IC供电,不用锂电池的top cell电压。Datasheet中P10显示bq79616可应用于VCn-VCn-1为-2~5V情况。P14显示负压测试精度。
P10:
P14:
麻烦确认以下4个问题,谢谢。
1、若C2对Gnd_1的电压是0.5V,C1对Gnd_1的电压是2V,bq79616能否测出C2-C1的压差?
2、若C2对Gnd_1的电压是0.5V,C1对Gnd_1的电压是4.5V,bq79616能否测出C2-C1的压差?

3、只要VCn-VCn-1满足-2~5V应该都是可以测的吧,不然规格书P10里面应该不会写-2~0V这段区间,同时P14不会把-2~0V的精度写出来?
4、Datasheet中P14显示main ADC负压精度,AUX_CELL无数据说明负压,那AUX_CELL能测负压吗?
P14: