This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS73225-EP: TPS73225DBVR输出电压为5V

Part Number: TPS73225-EP

如图所示,最下边的TPS73225DBVR(output type为fixed)的EN和IN我的输入电压是5V,但是NR通过电容接地和文档一致,但输出电压却是5V,但这个芯片的输出电压应该是2.5V才对

通过电笔测量,EN和IN都是5V,GND0V,NR约为0.2V,OUT为5V