This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS84259: 关于外接时钟CLK

Part Number: TPS84259

外接时钟给CLK管脚,是不是为了同步TPS84259的开关频率,避免开关噪声影响其他信号?还有其他用途吗?

另外CLK的电压范围是多少呢?根据手册12.10节,"The clock signal amplitude must transition lower than 0.5 V and higher than 2.2 V."

同时4.4节CLK High-Level Threshold和Low-Level Threshold  “with respect to A_VOUT”

This voltage rating is referenced to A_VOUT, not GND.

A_VOUT和VOUT短接(-8V),CLK要参考AVOUT吗?CLK范围是-5.8V?