Part Number: TPS92691-Q1
Other Parts Discussed in Thread: TPS92691
如果需要設計Vin = 9V~16V, ILED = 1.3A, 四晶LED(VLED = 12V), 此款IC是否合適呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS92691-Q1
Other Parts Discussed in Thread: TPS92691
如果需要設計Vin = 9V~16V, ILED = 1.3A, 四晶LED(VLED = 12V), 此款IC是否合適呢?
請問 IADJ VOLTAGE 與 RADJ1、RADJ2的關係是甚麼呢?該怎麼用RADJ1、RADJ2來算出 IADJ VOLTAGE?
如果RADJ2 = 100k ohm, 我想透過改變RADJ1, 來調整 IADJ VOLTAGE 保持在140mA~2.25V
HI
见datasheet第22页公式31, Vadj和LED电流的关系,如上设置Radj2,改变Radj1,保持Vadj电压在140mV~2.25V, 按照公式即可确认输出电压范围。
Hi
Radj1是先直接定一个值,然后用这个电阻计算Radj2。
没有计算工具,按照datasheet上案例设计即可,Q2是NMOS.
Buck-Boost 架構中, 按照datasheet , Q2是使用PMOS, 搭配Q3 = NOMS做使用, 想請問是否可以單一使用Q2 = NMOS, 直接接入DDRV, 而不使用Q3呢?
HI
你推到的电路是图26,还是图41, 建议按照图41设计,这里有详细的设计计算。 N-MOS和P-MOS的导通条件完全不同,需要按照参考电路来做。