Part Number: TPS54620
请教一个问题。我知道通过DAC输出接在FB端可以调节TPS54620输出电压,那么,如果让主处理器输出高频PWM波(20kHz),通过电阻连接到TPS54620芯片的FB端,从而控制其输出电压类似PWM波高低电压周期性输出的效果,让输出电压在0.8V和12V之间高频跳变。请问这种方案是否可行?我考虑到这么做会存在电压上升时间的问题,TPS54620的SS/TR端口连接的电容Css可以决定芯片软启动的电压上升时间Tss,在一般Css取10nF的情况下,输出电压上升时间Tss为3.5ms。显然这个电压上升时间太大了,PWM波的周期要远大于上升沿的,这样就无法做到高频PWM了。那么,我能不能把这个SS/TR端口的电容Css降低到很小,比如pF量级甚至更小,让电压上升时间变短,这样做对芯片有危害吗?会不会芯片内部构造就决定了这么高的频率控制下TPS54620芯片是无法快速稳定输出电压的?