This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25703A: BQ25703A

Part Number: BQ25703A

TI 工程师:

     你们好,我想问一下BQ25703A这个充电控制芯片的Vsys引脚的电压问题,我的问题点是当我整个系统长期没有工作,电池电量已经严重消耗至尽,此时我们如果对系统进行充电,对该芯片进行12V输入,Vsys系统默认输出为6V,6V电压不能给电池组(3串3并)进行充电,而且此时的6V电压不足以使得我们后端的MCU启动,因为我们给Vsys设置的电压是9V,只有当MCU启动后,该芯片才能使Vsys输出9V进而对电池组(3串3并锂电池)充电。因此我想咨询一下Vsys的系统电压默认值可以通过外围硬件电路修改到9V或者9V以上吗?非常感谢!

                     

  • Part Number: BQ25703A

    TI 工程师:

         你们好,我想问一下BQ25703A这个充电控制芯片的Vsys引脚的电压问题,我的问题点是当我整个系统长期没有工作,电池电量已经严重消耗至尽,此时我们如果对系统进行充电,对该芯片进行12V输入,Vsys系统默认输出为6V,6V电压不能给电池组(3串3并)进行充电,而且此时的6V电压不足以使得我们后端的MCU启动,因为我们给Vsys设置的电压是9V,只有当MCU启动后,该芯片才能使Vsys输出9V进而对电池组(3串3并锂电池)充电。因此我想咨询一下Vsys的系统电压默认值可以通过外围硬件电路修改到9V或者9V以上吗?非常感谢!

  • 您好,CELL_BATPRESZ设置3S,这样默认的VSYS_MIN就是 9216 mV。