Part Number: BQ24253
Other Parts Discussed in Thread: BQ25606
目前我使用的器件为BQ24253,通过Vsys为系统供电,输入电流限制为2A,充电电流也是2A,实测充电可以达到2A。设备的最大电流为1.8A(峰值),在设备的使用过程中,发现只插电池的情况下设备工作正常,负载工作情况良好,能达到最大电流值。但是只插适配器的情况下发现当处于峰值工作电流时,设备工作不正常(适配器5V4A)。下一版打算用bq25606,3A的电池管理芯片,请问这种带电源管理路径的电池管理IC在只插适配器的情况下是否能达到标称的电流,还是必须有电池才能达到。因为我想让我的设备即能用适配器独立工作,又能只用电池。
综上,为什么bq24253只插适配器的情况下Vsys带不动载,只插电池可以。还有就是更换bq24253是否可行。谢谢大家。