Part Number: TPS54561-Q1
请教一下,TPS54561-Q1在设计inverting电路时,它的Thermal pad是接GND还是接输出,SLVA317中datasheet并未提到这一点
另外常温测试负载在3A时IC温度大概有110℃,正常吗?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS54561-Q1
请教一下,TPS54561-Q1在设计inverting电路时,它的Thermal pad是接GND还是接输出,SLVA317中datasheet并未提到这一点
另外常温测试负载在3A时IC温度大概有110℃,正常吗?

HI
Powerpad在inverting电路时是连接到负压的,而不是0V GND.
芯片温度过高,首先需要确认Powerpad是否充分和PCB 铜箔充分焊接,并扩展散热(最好是四层板)。
110℃是偏高的,要看散热设计是否良好?