Part Number: TPS2491
怎么理解Tstart
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
主要看第一句来理解Tstart:
The fault timer runs when the hot swap is in power limit or current limit, which is the case during start-up. Thus the timer has to be sized large enough to prevent a time-out during start-up.
第一句翻译:“故障定时器运行当热插拔工作在功率限制或电流限制,即热插拔启动时“;故障定时器可以理解成是Ctimer?
我理解Tflt的时间就是出现功率限制或者电流限制后,芯片以25ua电流给Ctimer在第一个周期充电到4V的时间;然后tps2491又会持续15个周期充放过程;Tfit这个时间应该也就是故障定时器运行的时间吧?所以按照我的翻译,那故障时间的Tflt就应该和Tstart相等了?麻烦你看看我哪里理解错误;
HI
Tstart出现在start-up, 是此时功率或者电流限制的时间。
Tfit时间包括上面start_up的时间,应该是整个启动过程的时间,所以这个时间是要长于Tstart-up.
你好。我可不可以这样理解。因为我们tps2491,在startup时存在电流或者功率限制,会给Ctimer充电。如果在Ctimer充电未到4v的时候限制就消失了。那么给Ctimer充电的时间就是Tstart?相反,如果Ctimer充电到4v的过程限制一直没消失,那么这个时间就是Tflt。