This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A39: 关于TPS7A39的问题

Part Number: TPS7A39


大家好,我在使用双通道正负输出的LDO  TPS7A3901时,出现无输出的问题。

原理图如下:

PCB散热焊盘局部如下:

我这是4层板,散热焊盘是通过内层跟PIN4连接在一起的。可是3片样品PCB都没有输出。在断开负载后,故障依旧。测量输入的+/-5.5v都正常,各引脚焊接都正常。加大输入输出电容到100uF,也没有输出。加大输入电压到+/-6.5V也还是一样不行。

进一步测量BUF引脚和VNR/SS引脚也没有输出。因为原理图肯定没有问题,我怀疑是不是散热不行,造成内部温度太高而自动关闭了。因为散热焊盘只有三个国控打到内层pgnd,而前在内层连接的线也很细,看下图:

整个腹部散热焊盘只有红圈中的4各地方连接到内层PGND。

我想请教:

1、空载的情况下,片内的温度会上升到Tj>Tsd的情况从而芯片热保护而关闭吗?  Tj=室温25+功耗*55, 功耗应该很小啊,输入输出压差只有1V左右,输出又是空载,只有在反馈电组上有一点功耗,按道理应该不会出现Tj>180度的情况让器件自己关闭啊。。。

2、如果确实因为不良的散热,造成自动关闭,那我是否可以通过加散热片的方式让器件工作呢?

3、如果不是温度的原因,请教大家,还有什么可能性会导致器件不工作呢?谢谢!