This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7B4250-Q1: TPS7B4250QDBVRQ1客户电气性能测试出现引脚2未接地和引脚5未连接,请帮忙看下是否正常?

Part Number: TPS7B4250-Q1


您好:

     TPS7B4250QDBVRQ1 客户测试发现与数据不符,但我们能确定货是正规渠道的,原装正品,请问为什么会出现这种情况呢?

After electrical test, we found there are inconsistence between the test result and datasheet. We found pin 2 is open circuit in the curve trace.

Please help to ask for MFG explanation about why pin 2 is not connected to ground and not connected to pin 5.

Please see the attached pictures.
Test Condition:
when one pin was tested, all the other pins are grounded.
Range: from -1.5v to +1.5v
Sampling point : 100

下面是此型号的照片

  • Hi

       我想确认一下现在的不良模式是什么?  PIN2或者PIN5在PCB上接GND,  测试出来的异常是什么?(电压上)

       你们怎么确认的Pin2、Pin5没有接芯片内部的GND?

  • 你好,客户目前是想知道,这颗料,脚2是否与脚5内部连接?

  • 你好,以下是客户的回复:

    1,datasheet上写着pin 2 和pin 5是内部有连线的, 我们用两个探针测试pin 2 和 pin 5,发现是断路,我们不清楚内部连接是有
    其他的电路导致它们是断路还是因为没有导线连结导致的断路。

    2,我们没有用来测试的PCB板子
    3,我们实验室测试的层面是在把其他所有引脚接地的情况下,测试一个引脚的电压 vs电流,我们想了解pin2和pin5是否连接到同一个ground? Pin 2是否是一个单独的ground?

  • Hi

       从Datasheet Pin脚定义来看,芯片内部pin2和pin5是连接的. 但是芯片分2个脚来做GND,  不排除芯片内部分开隔离出2个GND, 并利用外部连接GND.

       所以才建议在PCB上电性测试确认。如果没有PCB,  LDO电路比较简单,在洞洞板上测试确认也是可以的。