This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV757P: 输出电流没有达到规格书中的1A

Part Number: TLV757P
Other Parts Discussed in Thread: LM3671

芯片使用的TLV75712PDBVR,SOT23-5封装,输入5V,输出1.2V,Lout输出没到1A,大概600mA,输出就被拉低了,想问一下可能是什么原因?

可能是因为过热吗?

然后换上LM3671,SOT23-5,就能正常工作。

想问一下

1.TLV75712PDBVR的结温有没有一个计算方法或者计算公式,按照手册8.2.2 Detailed Design Procedure吗?看手册有这样写的

Activating the thermal shutdown feature usually indicates excessive power dissipation as a result of the product of the (VIN – VOUT) voltage and the load current

2.LM3671,同样的输入和输出,是DCDC,就没什么问题,这个为什么?

谢谢。

  • HI
         5V输入,1.2V输出,600mA负载,芯片功耗为(5-1.2)*0.6=2.28w,    按照datasheet第四页热阻,你可以算一下芯片的结温,很可能已经超过芯片的热保护点。(功耗乘以热阻加上室温就是芯片的结温,所以LDO功耗较大的时候,要特别注意散热的设计,要尽量选择热阻较小的LDO芯片)

         类似LM3671的DC/DC, 和LDO不同,效率很高,芯片的功耗相对很小,即便热阻相对较大,芯片的温升也会很小。