Part Number: BQ20Z655
Other Parts Discussed in Thread: BQ40Z50, BQSTUDIO

在这个界面上,输入什么命令可以将电量计芯片解锁
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,现在SBS页面的ManufacturerAccess 框中输入密码看是否能解码,如果能解码说明密码是对的。
再到SMB 界面中的60地址连续输入密码试一下。
详细请参考TRM B.16 UnSealKey (0x60)
您好,从Unsealed模式变为Full Access,请在ManufacturerAccess 下两遍FFFF,FFFF试一下。
修改密码方法如下:
The unseal key can be read and changed via the extended SBS block command UnSealKey when in FULL ACCESS mode. To return to the SEALED mode, either a hardware reset is needed, or the ManufacturerAccess seal device command is needed to transit from FULL ACCESS or UNSEALED to SEALED.
您好,找到BQ40Z50修改密码的方法,您可以参考一下
I want to change Security Keys as "20180823" via Bqstudio.Advanced Comm SMB. Is below step 6~8 right?
At FULL ACCESS.
1. Key in Write Word command=00
2. Key in Word=0035
3. Click "Write Word" bottom.
4. Key in Read Block command=23
5. Click "Read Block" bottom to check default key is "14 04 72 36 FF FF FF FF".
6. Key in Write Block command=44
7. Key in Block command=35 00 18 20 23 08 FF FF FF FF
8. then click "Write Block" then go back to step 5 to check key.