Part Number: BQ25896
hi teams,
BQ25896的充电过压保护问题,此IC的充电OVP是硬件设置还是软件设置的,目前有看到在VBUS在6.7V时是停止充电,但是还是可以看到90MA左右的充电电流,想确认是不是BQ25896还在漏电。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,详细请参考数据手册9.2.15.1 Battery Overvoltage Protection (BATOVP)
The battery overvoltage limit is clamped at 4% above the battery regulation voltage. When battery over voltage occurs, the charger device immediately disables charge. The fault register BAT_FAULT bit goes high and an INT is asserted to the host.