This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS5430使用问题

Other Parts Discussed in Thread: TPS5430, TINA-TI

      各位专家好,我最近用tps5430。按照官网上datasheet上的电路图焊的。目的是输出5V的电压,负载上过大约2A的电流。焊好之后输出电压根本达不到5V。现在有以下几个问题:

    1、PWPD脚我是把转接板中间打了一个孔,然后把芯片肚子上的9脚接地的,还有那个ENA脚,在实际的焊接中是该接到VCC,还是地,还是悬空?datasheet中是这样说的:On/off control. Below 0.5 V, the device stops switching. Float the pin to enable.可是我试过好像都不能正常输出5V电压。

   2、原理图上画的电感应该是非线性电感,非线性电感和线性电感区别是什么?我实际中是用铁粉芯的磁环自己绕的,这个可以吗?还有那个B340A的肖特基二极管,我是用的1N5822,(百度上看到别人说可以代替的)

   3、再有就是关于TINA-TI仿真的,实际焊接不成功后,我试着用TINA仿真,在安装文件example我找到了官方对tps5430的仿真,可是我实际运行了以后,感觉输出的电压也不是5V,可能是我仿真的方法不对,我是先选择T&M->multimeter->然后点下直流电压那个按钮,测量输出就只有7.99nv.打开ENA那个开关后Vout就是3.51uv。附件是官方tina仿真的图

      

TPS5430 5V buck converter startup - autosave 13-05-12 19_41.TSC