输出电流2A 输入电压在16到24之间,输出分别为24,18,12,
请问专家如何选型芯片?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
请确认一下是不是三路输出都是2A。
如果是这样的话,建议使用UCC28600 QR反激或者UC2843 单管正激电源将输入升压至36V/3.5A
再使用三个TPS54240 BUCK电路分别产生24V/2A,18V/2A,12V/2A。