LM3881 adj 脚电容大小有限制么?SPEC上推荐是 10nf。 如果是 pf 级的电容,可以么?把时间限制在1ms以内
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LM3881 adj 脚电容大小有限制么?SPEC上推荐是 10nf。 如果是 pf 级的电容,可以么?把时间限制在1ms以内
Trevor 说:it can be shown that the timing capacitor-clock period relationship is typically 120 µs/nF. For example, a 10 nF capacitor sets up a clock period of 1.2 ms。
1nF的话,就是一个周期为0.12ms,假如9*0.12ms, 或者8*0.12ms可以满足你的时序要求,那也没有问题的。
Trevor回答得很好,补充一点就是电容的误差一般是20%,所以选在7nF比较合适。