This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于BQ2084的CEDV计算问题



老师,你们好!

想请教一个BQ2084 CEDV计算中遇到问题,在使用动态EDV0时候,如何看EDV0对应的电压点?是否是容量到0%时候对应的电压点?另外,如果使用的是固定EDV0,请问下固定的EDV0是在哪里设置?二者有何利弊?我应该怎么选择?

  • 动态的EDV0也是在固定的EVD0的基础上计算得到的,固定EDV0是RELATIVE STATE OF CHARGE为0%时对应的电压。

    如果要使用固定的EDV,那么CEDV bit in Gauge Configuration DF 0x29 要清零。

    相关设置的地址请参考如下内容

    Fixed EDV thresholds must be programmed in EMF/EDV0 DF 0x95-0x96, EDV C0
    Factor/EDV1 DF 0x97-0x98, and EDV R Factor/EDV2 DF 0x99-0x9a.

    以前的芯片都是使用固定的EDV技术的,后面才发展为有补偿的CEDV技术,补偿过的CEDV计算的精度更高,与固定版本相比更加符合电芯的真实状态。