我想做一个对两节锂电池电量检测的系统,并且在数码管上显示出来,请问哪款芯片比较合适呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
那么要参考30脚的BQ20Z60-R1,电量计一般都是1节电池的,或者适用于4节以下的,没有专门2节电池的应用。
http://www.ti.com.cn/product/cn/bq20z60-r1
http://www.ti.com.cn/lsds/ti_zh/power-management/battery-fuel-gauge-products.page
能说明下你所要做是什么样的应用?单片机是用来实现什么的控制?电池除了给单片机供电,还给什么器件供电?
如果给单片机供电的,200mA不知是否足够??
6.8V到8.4V的供电,转成5V的应用,最好还是选用DC/DC:
比如TPS62170
请问BQ20Z40可以测量7.2v-8.4v的锂电池电压吗?它提供的负载有多大呢
昨天我查了下,用bq26500可以检测8.4V锂电池的电量吗,这个给单片机5v的供电有什么好焊接的芯片吗?
BQ20Z40不建议使用,但BQ20Z40-R1可以,但需要跟bq29330结合使用。
这只是电量检测,不存在能提供多大的负载。7.2V-8.4V的电池电压还是需要通过降压电路转成5V,才能供单片机供电。能提供多大的负载在于电池及降压芯片。
TPS62170是能够提供最高0.5A电流输出的,如果电流还不够的话,可以使用TPS62160等
iverson allen 说:请问BQ20Z40可以测量7.2v-8.4v的锂电池电压吗?它提供的负载有多大呢
iverson allen 说:昨天我查了下,用bq26500可以检测8.4V锂电池的电量吗,这个给单片机5v的供电有什么好焊接的芯片吗?
好像BQ26500还是单电池的电量检测芯片;
http://www.ti.com.cn/cn/lit/ds/symlink/bq26500.pdf
手册里面有写检测电压范围为: