Part Number: TPS55288
芯片供电12V输入,使能端无效时通过I2C发送器件地址,器件无ACK应答信号,使能端有效时,输出为0.8V电压缓慢上涨为3.85V停止并保持稳定
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS55288
芯片供电12V输入,使能端无效时通过I2C发送器件地址,器件无ACK应答信号,使能端有效时,输出为0.8V电压缓慢上涨为3.85V停止并保持稳定
HI
确认I2C时序.(一般无法写读都是因为时序问题)
时序也无问题,逻辑分析仪住过波形,也试过软件模拟I2C或者硬件I2C都测试过,仅仅是器件无ack回复,其余都正常,外部上拉电阻10k,3.3V电压
Hi
如果时序,赋值都没有问题,所有板子都这样?做了多少板子?
HI
芯片哪里买来的? 建议找你们长期合作的渠道商买,如果是电子市场或者淘宝网站之类,很容易出现芯片质量问题。
Hi
1.2V以上为高电平,0.4V为低电平。
所以3.3V是可以的,你可以通过上拉电阻增加驱动电流看看。