This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

技术咨询

推荐个PMIC 至少4Buck输出,1LDOBuck可以输出5A意思(可以是合路之后),尺寸7mmx7mm以内,输入电压5V12V都可以,输出电压是可调节的。

 

补充需求

DC-DC:有1路最大输出5A以上,其余32A以上; LDO输出0.3A以上 电压最大可以支持3.3V,如果不行考虑最大支持2V