请问LM1085(to-263)的2针和4针都是5V输出么,有什么区别,设计PCB时,滤波电容最佳位置是哪?非常感谢~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
见datasheet第十二页说明: (内部连接)
It is important to remember that the TAB of the LM1085IS package is internally conntected to device pin 2 (OUTPUT)
输出电容,需要尽量靠近芯片脚。
紧接的一句“The copper area connected to the TAB can be left floating, used as the primary VOUT connection, or connected to
device pin 2 (OUTPUT) .”
所以TAB是可以当主输出用的。