Other Parts Discussed in Thread: BQ24140, BQ24618
我想做一个USB给手机充电的时候有个LED提示充电了 这样的一个方案
有什么管子可以解决吗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
单节锂电池的,是多少 毫安时的?需要多少A的充电电流?需要支持适配器与USB双输入的?满足所提要求的芯片有很多,比如BQ24140, BQ24618等,
http://www.ti.com.cn/cn/lit/ds/symlink/bq24618.pdf
http://www.ti.com.cn/product/cn/bq24192
zxjqq361 说:就是我们普通的USB下载线, 也可以给手机充电,,,插上手机的时候我希望USB的5V不受元件压降影响 ,,我想直接通向手机,,当手机充电的时候USB是4.7V了 (只是一根USB线)
然后外加电路,4.7V的时候LED亮提示 就可以了
所以也不是通过和手机通讯获得充电提示,只是测量USB线上压降判断是否在充电。
那就可以试试监控芯片TPS3824-50,RESET端接一个限流电阻,再接LED到地就可以了。TPS3824-50门限在4.55V,所以USB线上还要串些电阻。类似也可以用电压基准+电压比较器实现。
另外好奇问一句,如果电池快充满了,电流减小,压降减小,线端电压比4.7V高了怎么办?以前看过类似产品有些是有和手机通讯的,当然价格也不便宜。