在EVSW对电池组的检测中Fuel Gauge是使用那些数据计算出来的?
18650单个3.7V锂电池一般放电截止电压在2.8V,为什么在EVSW中Cell Voltage在3600mV左右时Fuel Gauge就只有0%啦?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
相关参数有电池的OCV-DOD曲线,电池内阻,截止电压,保留容量,负载选择(load select load mode)以及该参数使用到的电流或者功率值,最大化学容量。
针对你的现象可以检查下:
1.温度是否是低温,检查下截止电压保留容量等参数设置,放电截止电压这个是根据系统能够运行的最低电压来设置,需要在dataflash里填写
2.选择合适的CHEM-ID
3.golden learning
4.是否有过脉冲或者大电流放电
5.3600mV是否是放电到截止电压后静置读到的数值
如果还有问题可能需要继续检查下gg文件和log数据。谢谢!