This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于电源分压



在给一个场效应管供电时,想检测供电的电压值,于是通过两个普通的色环电阻分压给AD检测,但是当我输入的电压不同时,分压之后用示波器看到的电压值与衰减倍数有误差,而且输入的电压越大,误差越大,下面是一些数据,H4输入10.1V时,H1电压为903MV(衰减11.18);H4输入15.2V时,H1电压为1.37V(衰减11.094);H4输入20.5V时,H1电压为1.80V(衰减11.388);同时输出有80mv左右的噪声,这是为什么?有没有其他的解决方法,像π型衰减,或者其他的