This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq26500可以用来测量两节锂电池(7.2v-8.4v)的电量吗?电路中的RS电阻的阻值是0.02欧,这个用什么型号的,有什么特殊要求吗?

Other Parts Discussed in Thread: BQ26500

bq26500可以用来测量两节锂电池(7.2v-8.4v)的电量吗?电路中的RS电阻的阻值是0.02欧,这个用什么型号的,有什么特殊要求吗?

  • 应该BQ26500还是单节锂电池的电量检测芯片,检测电阻可用0.01或者0.02的. 具体型号可参考EVM板上的:

    http://www.ti.com/cn/litv/pdf/sluu174 第11页的R8

  • 如果你的电池精准度要求不高,可以加运放改为2S的方案,只是BQ26500报告的还是单节的电压,你在系统端处理一下,变为2S的电压。你说的电阻是精密电阻,要求精度为1%。

  • TI提供的比较简单的实现2S的方法是BAT脚通过一个10K欧姆的电阻接两串电池的最低一串电芯的正极,使得BAT的电压在允许的电压范围内,再用一个LDO把两节电池的正极电压降压以后送给芯片的VCC即可。因为实际测量的电压只有一串电芯,所以EDV电压和充电终止电压需要系统端做一个换算得到两节端口的电压。

    sensor 电阻要选择高精度, 低温漂, 和低寄生感抗的类型实际型号见trevor提到的EVM板中的实际器件,在layout的时候尤其注意采用开尔文氏连接,旁边尽量不要打过孔, 不要有并行的流通大电流的trace。