用UCD3138电源开发,是用USB-TO-GPIO,还是
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
用UCD3138电源开发,是用USB-TO-GPIO,还是
Hi
用UCD3138电源开发,是用USB-TO-GPIO
这个是一个接口期间,用于连接PC与电源板的通讯设备,可以采用TI的数字电源软件FUSION_DIGITAL_POWER_DESIGNER (http://www.ti.com.cn/tool/cn/fusion_digital_power_designer) 对设计芯片做相关设计, 详细见EVM板USER Guigde的操作步骤。
Flash Runner没有用过,但是从其说明文档来看是可以支持UCD3138的开发,文档还介绍了其使用的步骤,详见如下:
http://www.ti.com/lit/an/slua654/slua654.pdf
另外,Flash Runner支持的TI设备可以从这个文档查到:

Hi
两者都是可以的, 前者推出比较早,所以看得比较多。
前者主要是基于接口的直接设置编写:he communication between the USB interface adapter and the host PC is via USB, while the communication between the USB interface adapter and the slave device(s) is via an inter-integrated circuit (I²C), SMBus, PMBus and/or general-purpose inputs/outputs GPIOs.
后者是基于闪存芯片的系统内编程:tandalone In-System Programmer for Flash-based microcontrollers and serial memories. FlashRunnerTM FR03
谢谢您的回复!!!那我就选USB-TO-GPIO了!看UCD3138的技术文档,好像不仅需要用这个GUI软件进行相关设计,而且还要用CCS进行编程, 但我没有找到相关的例程,网站上只看到个CCS5.2的例程,并且没有相关.h头文件,您知道哪能找到么?
Hi
如果你采用USB-TO-GPIO, 可以看一下如下文档:
基于 GUI 软件配置 UCD3138 数字电源 PMBUS 命令: http://www.ti.com.cn/cn/lit/an/zhca519/zhca519.pdf
UCD3138064 Programmer’s Manual: http://www.ti.com.cn/cn/lit/ug/sluuad8a/sluuad8a.pdf
是用CCS编写PMBus命令?不过固件的基本配置的例程没有么?
这个芯片是需要先用CCS编程,生成个.Xo文件,再用GUI吧
以下两个E2E的帖子供你参考一下-
http://e2e.ti.com/support/power_management/digital_power/f/184/t/237310.aspx
http://e2e.ti.com/support/power_management/digital_power/f/184/t/215754.aspx
CHAO FANG 说:谢谢您的回复!!!那我就选USB-TO-GPIO了!看UCD3138的技术文档,好像不仅需要用这个GUI软件进行相关设计,而且还要用CCS进行编程, 但我没有找到相关的例程,网站上只看到个CCS5.2的例程,并且没有相关.h头文件,您知道哪能找到么?
另外还有关于 UCD3138PFCEVM-026 and UCD3138OL64EVM-031 这两块DEMO的例程可以参考一下这个帖子,希望对你有帮助-
http://e2e.ti.com/support/power_management/digital_power/f/184/t/247812.aspx