Part Number: LM2841
我在使用LM2841进行电路设计时,发现部分芯片其Vfb与规格书不一致。原理图取自规格书中Vout3.3V的典型电路。部分板子正常输出,部分板子输出偏低。大概2V。经测量Vfb电压低。请问可能是什么原因?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
FB电压是输出电压通过反馈分压电阻分出来的,所以输出偏低,自然会导致FB偏低。
输出电压偏低,你可以确认一下是否功率电感饱和(可以更换电感看看,或者减小负载看输出电压是否能正常输出3.3V)
其次可以将layout放上来看一下,layout不好如功率回路太大,可能导致带载能力降低,当输出电流偏高时过载保护也可能导致输出电压偏低。
最后确认一下输入电压是否有拉低的情况?