Part Number: BQ4050
BQ4050的两串项目,采用CEDV算法,GPCPackaged-report报告误差丢是在范围之内,(低温是做的-20℃),验证时在常温下循环两3次数据正常,无跳变,在常温下充满,-20℃下放电,电压到0%电压点了,但是soc只放到14%,到不了0%4657.GPCPackaged-report.zip
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: BQ4050
BQ4050的两串项目,采用CEDV算法,GPCPackaged-report报告误差丢是在范围之内,(低温是做的-20℃),验证时在常温下循环两3次数据正常,无跳变,在常温下充满,-20℃下放电,电压到0%电压点了,但是soc只放到14%,到不了0%4657.GPCPackaged-report.zip
您好,低温需要多做几个循环因为需要根据负载和温度(但不能低于-20C)调整EDV2/1电压,以缓解SOC跳变。
The bq4050 uses CEDV, which relies on accurate learned FCC with qualified discharges. See 6.3 in the TRM for details. A qualified discharge to update FCC has, among other rules, a limit on temperature, which is 11.9C by default. A battery will have vastly reduced capacity at -20C and depending on the load, FCC can be significantly less than FCC that was learned above 11.9C. Therefore it is possible that the gauge will calculate incorrect SOC at -20C because it will use FCC that is too high for this temperature. There is a limitation of the CEDV algorithm.
If you observe a jump in SOC at room temperature then the previously learned FCC is not indicative of the conditions that were present. For example, the load may have increased. That's why it is important for the gauge to learn FCC through regular discharges with a typical load at temperatures above 11.9C.
我现在是在常温下充满放空更新新的FCC,再在常温下充满在低温-20℃下放电,因是常温下更新出来的FCC是常温下的容量,电芯在低温下容量会有20%左右衰减,循环有最低温度11.9℃更新要求,所以低温-20℃不会更新FCC,两个容量相差太大会导致末端跳变,客户现在也是这样验证,就像您回复的有这样的问题,那么此问题如何解决?就是多做循环,需要在什么条件下做循环,才能最终保证在-20℃下不会有跳变,谢谢!
放电率是客户要求的,没法做更改,客户也会按这个电流验证的,我看有说低温建议调TC值,但是不知道调多少合适,算出来的是11,我调0后,到更新点后SOC会跳,不改TC值soc会一直减小,到0点电压点也不会跳0,应该是补偿的EDV值减小了但是怎么解决这个问题啊,主要是低温FCC偏大,EDV值偏小