Other Parts Discussed in Thread: OPA380, MC34063A, LM2663, TPS60500, TPS54160, TPS54040
我想用两片mc34063a产生正负2.5v的电压,电流几十毫安(供电opa380),输入电压可以是+5v吗?
如果不行的话,应该是多少?
还没有其他的芯片可以产生正负2.5v供电opa380?
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
mc34063a是可以做降压转换以及负压转换的,能够实现你的设计要求+/-2.5V。
因为你的电流需求比较小,或者可以采用2个chargepump芯片来做:
先用TPS60500 将5V转换成2.5V, 再用LM2663将2.5V转换成为-2.5V.
见如下芯片官网:
http://www.ti.com.cn/product/cn/tps60500
http://www.ti.com.cn/product/cn/lm2663
或者用TPS54040设计,可以参照同类芯片TPS54160的设计文档:http://www.ti.com.cn/cn/lit/an/slva369a/slva369a.pdf 用一片芯片通过耦合电感同时产生+/-2.5V.
可以用LM1117-2.5来产生+2.5v,再用LM2663将2.5V转换成为-2.5V?
Hi
5V到2.5V的转换可以用DC/DC, LDO, chargepump, 如果用LDO效率50%没有问题的话,可以用LM1117-2.5,
也可以用小电流的LDO, 如TLV70025: http://www.ti.com.cn/product/cn/tlv70025 等,成本也比较低,但是如果你2.5V还会带其他负载,是可以选择较大电流的LDO如LM1117-2.5.