Part Number: BQ25703A
Other Parts Discussed in Thread: TIDA-050047
TI 工程师:
你们好,我想问一下BQ25703A这个充电控制芯片的PD功能,因为我看规格书书上是这样写的:
(1)从各种输入源为1 至4 节电池充电的时候支持USB2.0//3.0/3.1/PD的输入电流设置。
(2)从电池给USB 端口加电(USB OTG)
– 输出4.48V 至20.8V 与USB PD 兼容
– 输出电流限制高达6.35A。
因为我现在想用type_C接口通过这个bq25703a给电池充电,看能不能使用市场上常用的PD功能的适配器给快充,但是这个芯片的配置上我没有看见CC1和CC2信号的接收引脚,所以这个PD功能给电池充电的时候是如何实现的呢?非常感谢!!!