Part Number: TPS61169
在使用TPS61169,原来的背光电流需要120mA,电阻只接了1.6R,PWM频率设置的18.7K,亮度调到最大时,Vbf测量204mV,现在背光电流最大需要260mA,电阻1.6R,有并联了一个1.3R的电阻,亮度调到最大时,但是测量Vbf只有约136mV,也就是背光亮度只能到190mA左右

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
是否有因为改变输出电感而确认功率电感饱和电路是否足够,而更换更高饱和电流的电感?
在负载变化时,建议对电路做相应的调整。