Other Parts Discussed in Thread: LP2985

LP2985AIM5-3.3由DCDC输出5V提供5V输入电源,且5V输入端有一个SMBJ5.0A的TVS管,输入电容1uF/50V(陶瓷电容,下同),输出电容2.2uF,BYPASS旁路电容10nF/50V,ON/OFF上拉100K电阻到VIN,负载电流在1-50mA之间。
出现的故障现象:
1、在刚开始是正常的,使用一段时间(半个月到一年不等)后出现输出电压2V-2.8V左右,EN引脚电压低于2V
2、概率性发生。
3、纹波噪声很大。
维修测试:
1、测试过输入电源波形无过冲,测试过负载电流也无过载
2、将故障芯片的输入输出电容加大,输出电压还是不正常。
3、将ON/OFF上拉电阻改成10K,有些刚开始输出正常测几个小时后就不正常了
4、将ON/OFF上拉电阻改成1K或者0R,有些输出电压正常了,但有些还是不正常,即使正常输出的,ON/OFF输入电流也比规格书上标注的电流大。
疑问:
1、上述LP2985烧的原因是?
2、输入输出电容值如果未达到最低稳定输出电压的要求值时LDO是会烧,还是只是输出振荡不稳定?
3、规格书上ON/OFF接5V时,该引脚电流最大是15uA是指,该脚在外接5V时内部漏电流的最大值还是外部流入的电流不能超过15uA