设计中PWM有超过10ms低电平,会使芯片休眠,故需要EN一直为高,而后的LED用PWM 控制MOS管,应该如何调整设计使得EN一直为高时,LED通路能用另一路PWM信号控制,datasheet中参考设计是EN信号和控制LED通路的MOS管一致,如需要不同信号,如何调整电路实现,多谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
不太明确你的意思,你需要时PWM控制EN脚电压一直为高,但是PWM信号中有10mS的低电平,然后需要忽略掉这个低电平,让芯片EN一直为高吗?
Hi
这个电路不需要给2个PWM, 要么你选择用EN脚PWM输入做调光,这个时候不要Q1的调光电路。 或者EN一直为高, 然后PWM输入Q1做调光。
HI
EN一直为高,PWM输入Q1是可以的。 这个时候FB电压并非正常FB电压,而是因为输出随PWM不停开关导致LED变暗。(此时等效亮度就是0.1V/R3)
Hi
PWM控制的是输出电压不停的on和off, 所以这个时候反馈并非正常的0.2V(理论上on的时候是0.2V, off的时候是0V, 不停的on和off,按照占空比来对应中间的电压)
HI
前面提到“设计中PWM有超过10ms低电平,会使芯片休眠”, 这个是系统给的信号,对于TPS61500而言, EN信号,或者Q1的PWM都不会有这个要求。