Other Parts Discussed in Thread: LMV7219
我使用CD4011的两个与非门构成一个RS触发器,来实现我的滞环控制,电路图如图所示


但是发现输出不正常,并没有像RS触发器那样工作,输出是这样

1通道是Q,2通道是R,3通道是S。

并且Q和Q非也不是互补的,如图所示。
不知道是什么原因造成的,信号频率大约是100khz-400khz
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,RS触发器使用与非门构建是没问题的。 并且看CD4011的电路也是没问题的。
前端比较器LMV7219,接了1nF的电容到地,相当于接了负载电容,可以看下负载电容和传输延迟的关系,容值越大,传输延迟越大。建议将C6和C15去掉试试。

其次,CD4011这颗逻辑器件应该很老了,我看数据手册还是影印版的,断开LMV7219,先验证CD4011的与非逻辑是否没问题,如果没问题,然后给RS逻辑高低电平看是否能正常输出?