This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS659037: 电压输出7.19s之后电压之后LDO_VRTC由1.797-1.692V,其他电压为0.

Part Number: TPS659037
Other Parts Discussed in Thread: AM5728

您好:

     1.  问题是:采用的电源管理芯片TPS6590376ZWSR,MCU是AM5728,目前出现的问题是上电7.19s之后电源管理芯片引脚F8由3.29V变为0.57电平,通过电源管理芯片的除了LDO_VRTC由1.797-1.692V,其他通过电源管理芯片出来的电压都为零,请问哪里出了问题。

2.与TI设计有一个模式不同,BOOT0,BOOT1设置不同,资料中BOOT0为低,BOOT1为高电平,设计的BOOT0和BOOT1是都为低电平,手册中没有说明BOOT设计的区别,测试表格如下,请协助解决谢谢。

序号 引脚 NET 相对于PIMC输入/输出 测试点位置 应该测试到的值 测试结果
1

B9

VUSB_3V3 O TP10
3.3V
3.279-0
2 A8 LDO_VRTC O TP11
1.8V
1.797-1.692
3 C6 VDD_SD O TP13
3.3V
3.299-0
4 B6 VDD_SHV5 O TP14
3.3V
3.282-0.165
5 K11 VDDA_1V8_PHYA O TP15
1.8V
1.794-0
6 K12 VDDA_1V8_PHYB O TP16
1.8V
1.793-0
7 A5 VDD_RTC O TP17
1.0V
1.046-0
8 B5 VDDA_1V8_PLL O TP18
1.8V
1.791-0