This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3447 如何能实现恒功率控制 怀疑

Other Parts Discussed in Thread: LM3447

LM3447的pdf读了3-4遍,没有看出来怎么实现恒功率控制的。其实Ti公司或者说是NS的想法是很不错的。

Pin<avg>=Vin<rms>*Vin<rms>/Re,其中Re=2*Lm/(D*D*Ts),也就是说当Lm确定,Ts确定,输入功率只和Vin<rms>和D有关。

即Pin<avg>=k*(Vin<rms>*D)*(Vin<rms>*D)。所以引入了电网电压前馈信号,抵消D的变化,实现输入恒功率,即输出恒功率。

当Vin<rms>升高k%时,电网电压前馈信号使得D降低k%。

但是很遗憾在Ti的pdf上没有看到控制环路上的处理。下图是TI给出的前馈控制框图:

图中,Vac引脚采样整流后电网电压波形,得到Iac。iac/10=iFF电流。iFF电流经过Cff和Rff滤掉100Hz纹波后,得到代表了整流后电网电压的平均值。

FF引脚和INV引脚连在一起,跨导型误差放大器的内部基准为1V(当然可以通过调光信号等可以调节内部基准),补偿器为电容。

疑问在于:1,这样接法,岂不是误差放大器的输出电压要么是恒为高电平,要么是恒为低电平,如何产生PWM波呢??

                   2,上图中,PWM的比较器的符号好像也有问题?图上所标为上+下-,但是我觉得应该是上-下+。

请高手解惑!!!!