有个项目用到LM2598这颗DC-DC,当输入接入12V~30V 时电路工作正常(输出电压为3.45V),当输入到36V~40V时,LM2598输入(VIN)输出(VOUT)直接击穿。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
有个项目用到LM2598这颗DC-DC,当输入接入12V~30V 时电路工作正常(输出电压为3.45V),当输入到36V~40V时,LM2598输入(VIN)输出(VOUT)直接击穿。
Hi
在你的电路图中没有看到输入电容, 按照datasheet建议:A low ESR aluminum or tantalum bypass capacitor is needed between the input pin and ground to prevent large voltage transients from appearing at the input.
请增加输入电容之后再测试,建议值120uF, low ESR aluminum or tantalum ,靠近芯片Vin脚
Hi
过压导致的,本身电压36~40V, 接近规格上限(45V), 如果启动时输入有一个很大的震荡就会到比较高的电压甚至高出45V, 需要一个较低ESR的电容来稳压,大小看你的负载,如果负载比较小,可以选择47uF, 大的话选择120uF.
Hi
可以用示波器测试空载启动时Vin,如果没有出现超过耐压值得电压,仍然导致芯片烧掉的话。
建议在TI网站上申请免费样片测试:http://www.ti.com.cn/tihome/cn/docs/homepage.tsp