Part Number: TPS23753A
hi 老师们,
客户用TPS23753A,设计12W输出,电压12V电流1A。
现设计发热严重。在输出2W时,芯片温度达到50℃以上,红圈中mos也达到67℃。
请帮忙建议如何改善设计。谢谢

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
R177是4.7ohm吗? 选择的MOS, 建议Rdson以及Qg都尽量小一些。
芯片的主要功耗是驱动输出,所以如上确认Qg, 另外就是看芯片PIN脚输入电压是否有过压的情况(不过因为MOS也发烫,建议先确认驱动和MOS)