Part Number: LM5175
0116.lm5175.pdf
我输入电压30V,根据FB引脚进行配置的输出电压应该是36V,但是我的输出却是68V左右在波动,并且我调节FB引脚的反馈电阻他的输出电压保持不变,仍是68V左右,请问这一般是什么地方出现的问题啊?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM5175
0116.lm5175.pdf
我输入电压30V,根据FB引脚进行配置的输出电压应该是36V,但是我的输出却是68V左右在波动,并且我调节FB引脚的反馈电阻他的输出电压保持不变,仍是68V左右,请问这一般是什么地方出现的问题啊?
Hi
如果输出的68V是大致稳定吗? 是否是稳定的很可能是芯片FB脚损坏,可以先测试一下FB脚阻抗看看,或者更换芯片确认?
如果输出严重的不稳定,确认一下FB是否受到哪里的干扰或者是被异常的拉低?