This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R3-DEVICE-FW: GPIO功能

Part Number: BQ40Z50-R3-DEVICE-FW


看了数据手册,LED不需要用的时候会作为普通GPIO。

这里有个疑问,为什么要将LED功能跟GPIO分开呢?LED功能不就是用GPIO实现的吗?单独留GPIO有何用处?谢谢

  • 您好,GPIO and LED functionality cannot coexist: It is not possible for some pins to function for the gauge LED operation, while others are used as GPIOs. However, when the pins are used as GPIOs, the user can attach an LED and control the pin manually using the commands described below.