This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25703A: 将电池供电改为外部DC12V供电是否可行?

Part Number: BQ25703A

产品定义供电有两种方式,由TYPEC供电或DC 12V供电,任意一种供电或两种同时存在时系统需要正常工作,当DC12V供电时,TYPEC接Device设备如U盘,能向TYPEC输出5V供电。

咨询:

1、如将BATT端接DC 12V供电,连接到DC座上,能否完全替代电池供电,实现设备双电源供电,同时支持 TYPEC5  V OUT功能?目前我们另外一款平板用这个充电IC功能已经全部验证成功。

2、如果能实现,软硬件上需要做什么变更?目前有没有有人这样使用?

3、有无其它更好的方案提供?

感谢 支持,谢谢。