Other Parts Discussed in Thread: BQ78350, BQ76920, BQ24610, BQSTUDIO
1、项目的方案是瑞星微平台,cup通过sumbus与bq78350进行连接,bq78350与bq76920之间是I2C连接,控制4节18350电池,充电IC为bq24610 2、目前出现的问题是,充电快到100%红灯会闪烁(正常充电过程中红灯常亮,100%红灯灭,绿灯亮),概率性问题,这个主要最根本问题是充电和放电来回交替导致的,硬件上led灯是接到了充电IC bq24610的stat1引脚,主要是78350控制76920对电池的检测有问题导致来回充电,进而现象为灯闪烁 3、我们抓到用bqstudio单独给78350+76920+24610控制模块充电,不带有CPU。log名为平衡充开启100%红灯闪烁.log 4、目前我们把平衡充关闭、调整78250的充电截止电流低于210mA均能复现(BQ24610的截止电流是210mA,BQ8350的充电截止电流默认为250mA) 5、yunhu-zhuban-v03是原理图
ps:这帖子上面插入不了附件,附件在 案件編號: CS1093080,请帮忙看下,谢谢