使用LM5022做一个18-36转8V 2A的反激电路
目前空载下输出电压稳定的,但是一旦带载后输出电压就会掉到2V附近,想问下从哪几个方面去查找问题呢,变压器原边:辅助:副边为 1:2:1.5
变压器的功率能适应40W
原理图如下
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用LM5022做一个18-36转8V 2A的反激电路
目前空载下输出电压稳定的,但是一旦带载后输出电压就会掉到2V附近,想问下从哪几个方面去查找问题呢,变压器原边:辅助:副边为 1:2:1.5
变压器的功率能适应40W
原理图如下
Hi
变压器是厂家绕的,还是你们自己绕的,如果是后者有没有做相应的测试(例如确认其能做到40W)
其次波形上测试,有没有确认cs脚电压?(能否将波形放上来看看)
变压器是厂家做的,40W是可以的,目前部太确定是否为变压器的问题
测了下空载和0.5A负载下的CS引脚波形,如下:
空载下输出8V都是正常的
空载下VCC引脚波形:
0.5A下VCC波形:
手册上VCC电压范围应该是6.5~7.4V,但空载下就超过这个范围,但输出电压正常
带载后就输出不正常
这个问题是变压器的问题还是从哪个方面查?
还想请教下LM5022最大占空比90%,可以使用到90%左右吗,还是建议低于50%使用
谢谢
HI
我感觉是变压器问题,有没有问厂商是否有做对应测试?
一般设计建议50%duty以内。