bq24630rger做一个电源管理电路,输入15.5V10A的电压,电池采用4串,给电池的充电电压设定的是14V200mA,充电正常无问题。输出端我接的是一块电路板,电路板不需要电流的时候输入端的电压给电路板供电,当电路板工作需要电流的时候bq24630rger会切换电池给电路板供电,请问这个问题有没有大佬遇到过,求解答。(我的目的是像笔记本电脑那样实现智能切换,当没有电源插入时是电池供电,当电源插入时是电源供电而不是用电池的电,是不是这颗芯片不能实现这个功能。)急急急!求解答。
搜索
复制
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,带有电源路径的电池充电器会自动切换适配器和电池
BQ24630 sense the SRN as the battery voltage and the VCC as the adaptor voltage. If the voltage at VCC is not high enough above the voltage at SRN, the charger is in SLEEP mode - please refer to the SLEEP comparator spec for details. When the charger is in SLEEP mode, the battery powers the system through the BATFET. Once the adaptor voltage at VCC reaches the threshold and the SLEEP mode has been exited, the adapter power is connected to the system through the ACFET.
There is a break-before-make logic that keeps the ACFET and the BATFET off for 10 us to prevent shoot-through current. The gate drive provides fast turnoff and slow turn on to allow soft start upon switching either FET.