This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS5430: 輸出電壓不符設計,PH腳位沒有開關波行,維持在DC8V

Part Number: TPS5430

原理圖與PCB如下,輸出電壓8V(正常應輸出5V)

示波器量測PH腳位得到DC8V的結果,沒有正常切換,而且IC會發熱(約60度)。

實際輸出電壓7.9V負載電流60mA,電源供應器輸入24V,80mA,似乎有20mA在消耗?

把芯片換到其他板子(layout不同)可正常工作,芯片應該沒有損壞,Layout上是否有其他沒注意到的?

補充說明:

在24V OFF -> ON時,PH(pin 8)腳位波行

在24V ON -> OFF時,BOOT(pin 1)腳位會出現以下波行

ENA腳位輸出正常的5V

VSENSE(pin 4) 電位 2V