Part Number: BQ4050EVM-561
Other Parts Discussed in Thread: BQSTUDIO
在EVM板子无输入静置时,在bqStudio显示界面上有-5mA的电流出现,这个电流是我进行learning不成功的原因吗?
如何使板子恢复到初始状态?
谢谢回答,新手不太懂这个,一个劲的踩坑。
若是使用单片机STM32可以收集这些数据吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: BQ4050EVM-561
Other Parts Discussed in Thread: BQSTUDIO
在EVM板子无输入静置时,在bqStudio显示界面上有-5mA的电流出现,这个电流是我进行learning不成功的原因吗?
如何使板子恢复到初始状态?
谢谢回答,新手不太懂这个,一个劲的踩坑。
若是使用单片机STM32可以收集这些数据吗?
您好,cell测量电压为4.17V,pack+-测得电压为3.84V,有压差是不是充电MOS关了导致的。
这个网站上有其他芯片的sample code您看一下是否能打开
您也可以看一下文档
SMBUS MADE IN SIMPLE
https://www.ti.com/lit/an/slua475/slua475.pdf?ts=1606101553430