This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ20Z95 pulse charge configration



when I configurate the BQ20Z95 data flash, i come accross  a problem. I can't understand the pulse charge mode .who can tell me the pulse mode how to operate?

data flash content as follows: 

Turn ON voltage  

Turn OFF voltage

Max ON Pulse Time

Min OFF Pulse Time

Max OFF voltage

Look forward to respose! Thanks!

  • 如果你是一般的锂离子电池即CV电压为4.2V,那么这几个参数的默认值就是可以用的.

    关于你对于pulse充电的问题,详细的pulse充电的流程解释如下,希望能有助于帮助你深入的理解

    1:首先明确这个pulse充电发生在CV阶段的末期,此时充电还在进行,CHGFET ON.

    2:芯片检测fast charge的计时器是否溢出,即FC-MTO是否溢出。如果溢出则进入到关闭CHG MOSFET的状态;如果没有溢出,则检测任意电芯电压是否大于MAx off voltage ,如果是则关闭CHGFET,如果没有则检测是否任意电芯电压大于turn off voltage,如果不是则返回到正常充电模式,如果是则开始将on pulse timer清零并开始计时,当on pulse timer溢出以后进入到关闭CHG MOSFET的状态

    3;当进入到CHGFET关闭的状态以后,检测是否任意电芯电压低于turn on voltage,如果有发现低于turn on voltage (变化的原因是因为前面的停止充电以后电芯内部温度以及PTC的变化导致电芯的端口电压成为相对的一个静态电压,所以电芯的电压会有一个跌落),则判断是否 off pulse timer溢出,如果溢出则将off pulse timer清零以后开始检测之前sensor电阻上采集到的电流是否小于设置的截止电流,如果小于,则进入充电完成的状态,如果不小于,那么将CHGFET打开并将FC-MTO继续计时。进入到1的状态。